SBOK044B December   2020  – December 2024 TPS7H4010-SEP

 

  1.   1
  2. 1 Abstract
  3.   Trademarks
  4. 2 Introduction
  5. 3 Single-Event Effects (SEE)
  6. 4 Device and Test Board Information
  7. 5 Irradiation Facility and Setup
  8. 6 Depth, Range, and LETEFF Calculation
  9. 7 Test Setup and Procedures
  10. 8 Destructive Single-Event Effects (DSEE)
    1. 8.1 Single-Event Latch-up (SEL) Results
    2. 8.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 9 Single-Event Transients (SET)
  12. 10Event Rate Calculations
  13. 11Summary
  14. 12Revision History
  15.   A Total Ionizing Dose from SEE Experiments
  16.   B References

Test Setup and Procedures

SEE testing was performed on a TPS7H4010-SEP device mounted on a TPS7H4010EVM. The device power was provided using the J19 (PVIN) and (GND) inputs with the N6766A PS Module mounted on a N6705 precision power supply in a 4-wire configuration. Discrete power resistors of 0.3 Ω (VOUT = 1.8 V) and 0.55 Ω (VOUT = 3.3 V) were used to load the device to 6 A for the SEE testing campaign. The device was tested under Auto Mode for all runs by tying the SYNC to GND using the J7 jumper.

For SEL, SEB, and SEGR testing, the device was powered up to the maximum recommended operating voltage of 32 V and loaded with the maximum load of 6 A. Two commonly used output voltages, 3.3 and 1.8 V, were used for the SEE testing campaign. For the SEB/SEGR characterization, the device was tested under enabled and disabled modes. The device was disabled by using jumper J6, connecting EN to GND. The discrete load resistor was connected even when the device was disabled to help differentiate if an SET momentarily activated the device under the heavy-ion irradiation. During the SEB/SEGR testing with the device in disabled mode, not a single VOUT transient or input current event was observed.

For the SET characterization, the device was powered up to 12 V for the 3.3-V VOUT case and 5 V for the 1.8-V case. The SET events were monitored using two National Instruments (NI) PXIe-5172 scope cards. One scope was used to monitor and trigger from VOUT, using a window trigger around ±3% from the nominal output voltage. The second scope was used to monitor and trigger from the PGOOD at 1.5 V (for the VOUT = 1.8 V) and 3 V (for the VOUT = 3.3 V), using a edge/negative trigger. Both scopes were mounted on a NI PXIe-1095 chassis.

All equipment was controlled and monitored using a custom-developed LabVIEW program (PXI-RadTest) running on a HP-Z4 desktop computer. The computer communicates with the PXI chassis via an MXI controller and NI PXIe-8381 remote control module.

Figure 7-1 shows a block diagram of the setup used for SEE testing of the TPS7H4010-SEP. Table 7-1 shows the connections, limits, and compliance values used during the testing. A die temperature of 125°C was used for SEL and was achieved with the use of a convection heat gun aimed at the die. For the SEB/SEGR testing, the device was cooled-down to ≈10°C using a VORTEC tube (model: 611), aimed at the die. For SET testing, the device was tested at room temperature (no cooling or heating was applied to the DUT). The die temperature was monitored during all the testing using a T-Type thermocouple attached to the thermal pad vias (on the bottom side of the EVM) with thermal paste. The thermocouple was held in place by using high temperature tape (kapton-tape). Die-to-thermocouple temperature was verified using a IR-camera prior to the SEE test campaign.

Table 7-1 Equipment Set and Parameters Used for SEE Testing the TPS7H4010-SEP
PIN NAME EQUIPMENT USED CAPABILITY COMPLIANCE RANGE OF VALUES USED
VIN Agilen N6700 PS (Channel #3) 15 A 10 A 5, 12, and 32 V
Oscilloscope Card on VOUT NI-PXIe 5172 100 MS/s — 10 MS/s
Oscilloscope Card on VOUT NI-PXIe 5172 100 MS/s — 50 MS/s
Digital I/O NI-PXIe 6589 — — Interrupt Based

All boards used for SEE testing were fully checked for functionality. Dry runs were also performed to ensure that the test system was stable under all bias and load conditions prior to being taken to the TAMU facility. During the heavy-ion testing, the LabVIEW control program powered up the TPS7H4010-SEP device and set the external sourcing and monitoring functions of the external equipment. After functionality and stability was confirmed, the beam shutter was opened to expose the device to the heavy-ion beam. The shutter remained open until the target fluence was achieved (determined by external detectors and counters). During irradiation, the NI scope cards continuously monitored the signals. When the output voltage exceeded the pre-defined 3% window trigger, or when the PG signal changed from High to Low (using a negative edge trigger), a data capture was initiated. In addition to monitoring the voltage levels of the two scopes, VIN current and the +5-V signal from TAMU were monitored at all times. No sudden increases in current were observed (outside of normal fluctuations) on any of the test runs and indicated that no SEL or SEB/SEGR events occurred during any of the tests.

TPS7H4010-SEP Block Diagram of SEE Test Setup With the
                                                  TPS7H4010-SEP Figure 7-1 Block Diagram of SEE Test Setup With the TPS7H4010-SEP. The lumped components in the block diagram represent the EVM set for VOUT = 1.8 V. For details on the EVM components regarding VOUT = 3.3 V, please refer to Figure 4-3.