SBOK044B December 2020 – December 2024 TPS7H4010-SEP
The heavy-ion species used for the SEE studies on this product were provided and delivered by the TAMU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1-in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For the bulk of these studies, ion flux of 104 and 105 ions/cm2·s were used to provide heavy-ion fluences of ≈ 3 × 106 and 107 ions/cm2.
For the experiments conducted in this report the following ions and corresponding angles were used in order to provide a range of LETEFF of 1.33 to 43 MeV·cm2 /mg.
Krypton (84Kr) at 44.3° for an LETEFF = 43 MeV
RangeEFF = 77.7 µm
Total Kinetic Energy = 2.081 GeV (25 MeV/nucleon)
Krypton (84Kr) at 42.7° for an LETEFF = 43.1 MeV
RangeEFF = 73.6 µm
Total Kinetic Energy = 1.259 GeV (15 MeV/nucleon)
Krypton (84Kr) at 0° for an LETEFF = 29.7 MeV
RangeEFF = 118.2 µm
Total Kinetic Energy = 1.259 GeV (15 MeV/nucleon)
Copper (63Cu) at 41.6° for an LETEFF = 28.1 MeV
RangeEFF = 80.1 µm
Total Kinetic Energy = 0.944 GeV (15 MeV/nucleon)
Copper (63Cu) at 0° for an LETEFF = 19.7 MeV
RangeEFF = 124.1 µm
Total Kinetic Energy = 0.944 GeV (15 MeV/nucleon)
Argon (40Ar) at 42.3° for an LETEFF = 12 MeV
RangeEFF = 120.8 µm
Total Kinetic Energy = 0.599 GeV (15 MeV/nucleon)
Argon (40Ar) at 0° for an LETEFF = 8.44 MeV
RangeEFF = 180.9 µm
Total Kinetic Energy = 0.599 GeV (15 MeV/nucleon)
Neon (20Ne) at 43.1° for an LETEFF = 3.89 MeV
RangeEFF = 177 µm
Total Kinetic Energy = 0.300 GeV (15 MeV/nucleon)
Neon (20Ne) at 0° for an LETEFF = 2.74 MeV
RangeEFF = 261.3 µm
Total Kinetic Energy = 0.300 GeV (15 MeV/nucleon)
Nitrogen (14N) at 0° for an LETEFF = 1.33 MeV
RangeEFF = 371.8 µm
Total Kinetic Energy = 0.210 GeV (15 MeV/nucleon)
Ion uniformity for these experiments was between 88 and 98%.
Figure 5-1 shows the TPS7H4010-SEP test board used for the experiments at the TAMU facility. Although not visible in this photo, the beam port has a 1-mil Aramica window to allow in-air testing while maintaining the vacuum within the accelerator with only minor ion energy loss. All through-hole test points were soldered backwards for easy access of the signals while having enough room to change the angle of incidence and maintaining the 40-mm distance to the die. The in-air gap between the device and the ion beam port window was maintained at 40 mm for all runs.
Figure 5-1 Photograph of the
TPS7H4010-SEP Evaluation Board Mounted in Front of the Heavy-Ion Beam Exit Port
at the Texas A&M Cyclotron