SBOA433 March   2021 TMP451 , TMP461 , TMP461-SP , TMP464 , TMP468 , TMP4718 , TMP4719 , TMP9R00-SP , TMP9R01-SEP

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Series Resistance
    2. 1.2 Variation of η-Factor
    3. 1.3 Variation of Beta
  3. 2Transistor List
  4. 3BJT Test Board
  5. 4Test Procedure
  6. 5Data and Recommendations
  7. 6Summary

Introduction

Remote temperature sensors measure the temperature of an external transistor by measuring the base-emitter voltage (VBE) of the BJT, which depends on temperature. One method of determining a transistor base-emitter voltage is the two current method, using the difference of two voltage measurements to calculate temperature, as shown in Figure 1-1. However, thermal diode signals can be sensitive to noise, series resistance, and variation in transistors’ η-factors and betas can introduce additional errors if not accommodated.

GUID-ED7CDC47-11FA-4568-99E5-B336190584B6-low.gif Figure 1-1 ΔVBE Measurement with Two Currents