ZHCS429J March 2012 – November 2021 UCD3138
PRODUCTION DATA
Figure 8-3 Power-On Reset (POR) and Brown-Out Reset (BOR)| TERM | DEFINITION |
|---|---|
| VGH | This is the V33D threshold where the internal power is declared good. The UCD3138 comes out of reset when above this threshold. |
| VGL | This is the V33D threshold where the internal power is declared bad. The device goes into reset when below this threshold. |
| Vres | This is the V33D threshold where the internal reset signal is no longer valid. Below this threshold the device is in an indeterminate state. |
| IReset | This is the internal reset signal. When low, the device is held in reset. This is equivalent to holding the reset pin on the IC high. |
| TPOR | The time delay from when VGH is exceeded to when the device comes out of reset. |
| Brown out | This is the V33D voltage threshold at which the device sets the brown out status bit. In addition an interrupt can be triggered if enabled. |