ZHCSI09S June 2010 – August 2018 TPS65911
PRODUCTION DATA.
The possible device reset domains are:
In the following register description, the reset domain for each register is defined in the register table heading.
NOTE
DCDCCTRL_REG and DEVCTRL2_REG have bits in two reset domains.
The comment Default value: See boot configuration indicates that bit default value is set in boot configuration and not by the register reset value.