ZHCSQ77A February 2023 – September 2023 TPS25948
PRODUCTION DATA
In the case of a short-circuit and overload current limit when the device interrupts current flow, the input inductance generates a positive voltage spike on the input, and the output inductance generates a negative voltage spike on the output. The peak amplitude of voltage spikes (transients) is dependent on the value of inductance in series to the input or output of the device. Such transients can exceed the absolute maximum ratings of the device if steps are not taken to address the issue. Typical methods for addressing transients include:
The approximate value of input capacitance can be estimated with the equation:
where
The circuit implementation with optional protection components is shown in Figure 9-23.