ZHCSDO6B May 2015 – September 2020 MSP430FG6425 , MSP430FG6426 , MSP430FG6625 , MSP430FG6626
PRODUCTION DATA
The following equations can give guidance on the input range for the CTSD16 while using an external reference. Keep in mind the absolute bounds of an external reference as mentioned in the specifications section of this module. The external and internal references cannot be used at the same time, because they share the same signal path and pin. For internal reference ranges, see Section 8.8.11.




Where
The differential input voltage range with internal voltage reference at different GAIN settings is given in Section 8.8.11. Using Equation 3 through Equation 6, determine the absolute maximum differential input ranges for the CTSD16 with a given external voltage reference. Equation 7 corresponds to the example circuit in Figure 10-6 and can be used after a range is chosen to limit differential input voltage to acceptable levels by solving for the external resistors R1 and R2.

Where