ZHCSN15B June 2020 – June 2021 LMK05318B
PRODUCTION DATA
The EEPROM array is non-volatile memory mapped directly from the SRAM array.
After the register settings have been written to the SRAM (by either Method #1 or #2), the EEPROM can be programmed through the following sequence:
On the next power up or hard-reset, the device can self-start in EEPROM mode from the newly programmed configuration. Also, the NVMCNT register value will be incremented by 1 after power up or hard-reset to reflect total number of EEPROM programming cycles completed successfully.