ZHCSDE3G February 2015 – October 2022 DP83867CR , DP83867IR
PRODUCTION DATA
请参考 PDF 数据表获取器件具体的封装图。
BIT | BIT NAME | DEFAULT | DESCRIPTION |
---|---|---|---|
15:8 | TDR_PEAKS_LOC_C_3 | 0, RO | Location of the fourth peak discovered by the TDR mechanism on channel C. The value of these bits is translated into distance from the PHY. |
7:0 | TDR_PEAKS_LOC_C_2 | 0, RO | Location of the third peak discovered by the TDR mechanism on channel C. The value of these bits is translated into distance from the PHY. |