ZHCSM59B November 2014 – September 2020 CC3100MOD
PRODUCTION DATA
The 3-wire UART topology requires only the following lines (see #SWAS0317491).
Figure 8-12 3-Wire UART TopologyUsing 3-wire topology requires one of the following conditions to be met:
Because there is no full flow control, the host cannot stop the SimpleLink device to send its data; thus, the following parameters must be carefully considered: