ZHCSD95D January 2015 – April 2021 BQ34Z100-G1
PRODUCTION DATA
The BQ34Z100-G1 is also capable of being used as a system-side gauge where the actual battery can be removed and replaced from the system. However, there are limitations to this feature. The replacing battery should be of the same chemistry and close to the original design capacity of the one to be replaced, as this ensures that the other configuration options of the device are still valid.
The BQ34Z100-G1 is enabled to have the option to learn new Impedance Track data in larger steps through the following configuration registers:
| Class Name | Subclass name | Parameter Name | Default Value | Units |
|---|---|---|---|---|
| Gas Gauging | IT Cfg | Max Res Factor | 50 | n/a |
| Gas Gauging | IT Cfg | Min Res Factor | 1 | n/a |
| Gas Gauging | IT Cfg | Max Res Scale | 32000 | n/a |
| Gas Gauging | IT Cfg | Min Res Scale | 1 | n/a |
| Gas Gauging | IT Cfg | Max QMAX Change | 100 | n/a |
If the BQ34Z100-G1 and the battery are not designed to be separated, it is recommended to make the following changes. This helps to prevent erroneous measurements from causing the Impedance Track data to be updated to extreme values.
| Class Name | Subclass name | Parameter Name | Value | Units |
|---|---|---|---|---|
| Gas Gauging | IT Cfg | Max Res Factor | 15 | n/a |
| Gas Gauging | IT Cfg | Min Res Factor | 3 | n/a |
| Gas Gauging | IT Cfg | Max Res Scale | 5000 | n/a |
| Gas Gauging | IT Cfg | Min Res Scale | 200 | n/a |
| Gas Gauging | IT Cfg | Max QMAX Change | 30 | n/a |