ZHCSG15A February 2017 – September 2021 TPL5110-Q1
PRODUCTION DATA
The TPL5110-Q1 can generate 1650 discrete timer intervals in the range of 100ms to 7200s. The first 9 intervals are multiples of 100ms. The remaining 1641 intervals cover the range between 1s to 7200s. Because they are discrete intervals, there is a quantization error associated with each value.
The quantization error can be evaluated according to the following formula:
Where:
REXT is the resistance calculated with Equation 1 and a,b,c are the coefficients of the equation listed in Table 7-1.