ZHCSG15A February 2017 – September 2021 TPL5110-Q1
PRODUCTION DATA
PIN | TYPE(1) | DESCRIPTION | APPLICATION INFORMATION | |
---|---|---|---|---|
NO. | NAME | |||
1 | VDD | P | Supply voltage | |
2 | GND | G | Ground | |
3 | DELAY/ M_DRV | I | Time interval set and manual MOSFET Power ON | Resistance between this pin and GND is used to select the time interval. The manual MOSFET power ON switch is also connected to this pin. |
4 | DONE | I | Logic Input for watchdog functionality | Digital signal driven by the µC to indicate successful processing. |
5 | DRV | O | Power Gating output signal generated every tIP | The Gate of the MOSFET is connected to this pin. When DRV = LOW, the MOSFET is ON. |
6 | EN/ ONE_SHOT | I | Selector of mode of operation | When EN/ONE_SHOT = HIGH, the TPL5110-Q1 works as a TIMER. When EN/ONE_SHOT = LOW, the TPL5110-Q1 turns on the MOSFET one time for the programmed time interval. The next power on of the MOSFET is enabled by the manual power ON. |