ZHCSDW8C April 2015 – December 2017 TPA3144D2
PRODUCTION DATA.
Changing the gain setting can vary the input resistance of the amplifier from its smallest value, 9 kΩ ±20%, to the largest value, 60 kΩ ±20%. As a result, if a single capacitor is used in the input high-pass filter, the -3 dB or cutoff frequency may change when changing gain steps.
The -3-dB frequency can be calculated using Equation 2. Use the Zi values given in Table 1.