The xWRL6432BOOST from Texas Instruments is an easy-to-use low cost FR4-based evaluation board for the xWRL6432 mmWave sensing device, with standalone operation and direct connectivity to the DCA1000EVM for raw ADC capture and signal processing development. This EVM contains everything required to start developing software for on-chip Hardware accelerator and low power ARM Cortex® M4F controllers.
ARM Cortex® is a registered trademark of Arm Cortex.
TI® is a registered trademark of Texas Instruments.
All trademarks are the property of their respective owners.
xWRL6432BOOST includes the following:
TI® provides sample demo codes to easily get started with the XWRL6432BOOST evaluation module (EVM) and to experience the functionality of the XWRL6432 mmWave sensor. For details on getting started with these demos visit mmWave SDK on ti.com page.
The XWRL6432BOOST includes three receivers and two transmitters with a wide field of view sitting on an FR4 PCB substrate.
Figure 3-5 shows the functional block diagram. The EVM contains the essential components for the TI mm-Wave radar system: DCDC, SFLASH, SOP configuration, Filter, TI mmWave Radar chip, a USB to UART converter, and a 60-pin Samtec connector for interfacing with the DCA1000. The board also hosts a booster pack connector which can be connected to TI’s LaunchPad boards.