SWRU596 December   2022

 

  1. 1Abstract
    1.     Trademarks
  2. 2Getting Started
    1. 2.1 Key Features
    2. 2.2 Kit Contents
    3. 2.3 mmWave Out of Box Demo
  3. 3Hardware
    1. 3.1 Block Diagram
  4. 4EVM Mux Block Diagram
  5. 5PCB Storage and Handling Recommendations:
    1. 5.1 PCB Storage and Handling Recommendations:
    2. 5.2 Higher Power Demanding Applications:
  6. 6XWRL6432BOOST Antenna
    1. 6.1  PCB material
      1. 6.1.1 Transmitter and receiver virtual array
    2. 6.2  Switch Settings
    3. 6.3  LEDs
    4. 6.4  Connectors
    5. 6.5  USB Connector
    6. 6.6  DCA1000 HD Connector
    7. 6.7  Booster Pack Connector for the LaunchPad Connectivity
    8. 6.8  CANFD Connector
    9. 6.9  LIN PHY connection
    10. 6.10 I2C Connections
      1. 6.10.1 EEPROM
    11. 6.11 XDS110 Interface
    12. 6.12 Flashing the Board
    13. 6.13 DCA1000EVM Mode
      1. 6.13.1 RDIF interface for Raw ADC capture
  7. 7Software, Development Tools, and Example Code
    1. 7.1 XWRL6432 Demo Visualization Getting Started
  8. 8TI E2E Community
  9. 9References
    1.     Revision History

Transmitter and receiver virtual array

Transmitter and receiver antennas positions in Figure 6-2 form a virtual array of 6 transmitter and receiver pairs. This allows object detections finer azimuthal angular resolution (29°) and coarse elevation angular resolution (58°). Receiver antennas are spaced at distance D (Lambda/2) and Transmitter antenna Tx1 and Tx2 spaced at 2D (lambda) in azimuthal plane and D (Lambda/2) in elevation plane. Tx1 and Tx2 are placed at D (lambda/2) in the elevation and 2D (Lambda) in azimuth plane.

GUID-74F6348B-C900-4EC0-B671-0875901E2748-low.png GUID-12045CAC-F9B0-4268-B297-1E4737CC4C7A-low.jpg Figure 6-2 Virtual antenna array

Figure 6-2 shows the antenna radiation pattern with regard to azimuth and Figure 6-3 shows the antenna radiation pattern with regard to elevation for TX1 and TX2. Both show the radiation pattern for TX1 and TX2 and RX1, RX2 and RX3 together. All of the measurements were done with a Tx and Rx combination together. Thus, for the -6dB beam width, you must see a -12db (Tx (-6dB) + Rx(-6dB)) number from the boresight.

Note: Wavelength (Lambda) is computed based on a frequency of 62GHz. Antenna placements are according to this frequency.
GUID-4B2CC1EF-64F2-4ADE-B609-B3384CF61799-low.png Figure 6-3 Azimuth Antenna Radiation Patterns

Measured azimuthal radiation pattern for all Tx to Rx pairs (Corner reflector placed at ~5 meters with a 4- GHz bandwidth chirp starting at 59GHz)

GUID-486EFFC6-2565-484B-BD3D-9FDDB31DA1B6-low.png Figure 6-4 Elevation Antenna Radiation Patterns

Measured elevation radiation pattern for all TX to RX pairs (Corner reflector placed at ~5 meters with a 4-GHz bandwidth chirp starting at 59GHz)

Note: In accordance to the EN 62311 RF exposure test, a minimum separation distance of 20 centimeters should be maintained between the user and the EVM during operation.