ZHCUBI3A November   2023  – April 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1

 

  1.   1
  2.   摘要
  3.   商标
  4. 1引言
    1. 1.1 参考书籍
    2. 1.2 函数清单格式
  5. 2TMS320F280013x/15x 闪存 API 概述
    1. 2.1 引言
    2. 2.2 API 概述
    3. 2.3 使用 API
      1. 2.3.1 初始化流程
        1. 2.3.1.1 器件上电后
        2. 2.3.1.2 闪存包装程序和存储体设置
        3. 2.3.1.3 关于系统频率变化
      2. 2.3.2 使用 API 进行构建
        1. 2.3.2.1 对象库文件
        2. 2.3.2.2 Distribution Files
        3. 2.3.2.3 Key Facts For Flash API Usage
  6. 3API 函数
    1. 3.1 初始化函数
      1. 3.1.1 Fapi_initializeAPI()
    2. 3.2 闪存状态机函数
      1. 3.2.1  Fapi_setActiveFlashBank()
      2. 3.2.2  Fapi_setupBankSectorEnable()
      3. 3.2.3  Fapi_issueAsyncCommandWithAddress()
      4. 3.2.4  Fapi_issueBankEraseCommand()
      5. 3.2.5  Fapi_issueProgrammingCommand()
      6. 3.2.6  Fapi_issueProgrammingCommandForEccAddresses()
      7. 3.2.7  Fapi_issueAutoEcc512ProgrammingCommand()
      8. 3.2.8  Fapi_issueDataAndEcc512ProgrammingCommand()
      9. 3.2.9  Fapi_issueDataOnly512ProgrammingCommand()
      10. 3.2.10 Fapi_issueEccOnly64ProgrammingCommand()
      11. 3.2.11 Fapi_issueAsyncCommand()
      12. 3.2.12 Fapi_checkFsmForReady()
      13. 3.2.13 Fapi_getFsmStatus()
    3. 3.3 读取函数
      1. 3.3.1 Fapi_doBlankCheck()
      2. 3.3.2 Fapi_doVerify()
    4. 3.4 信息函数
      1. 3.4.1 Fapi_getLibraryInfo()
    5. 3.5 实用功能
      1. 3.5.1 Fapi_flushPipeline()
      2. 3.5.2 Fapi_calculateEcc()
      3. 3.5.3 Fapi_isAddressEcc()
      4. 3.5.4 Fapi_remapEccAddress()
      5. 3.5.5 Fapi_calculateFletcherChecksum()
  7. 4推荐的 FSM 流程
    1. 4.1 新出厂器件
    2. 4.2 推荐的擦除流程
    3. 4.3 推荐的存储体擦除流程
    4. 4.4 推荐的编程流程
  8. 5与安全相关的软件应用程序使用假设
  9.   A 闪存状态机命令
  10.   B typedef、定义、枚举和结构
    1.     B.1 类型定义
    2.     B.2 定义
    3.     B.3 枚举
      1.      B.3.1 Fapi_FlashProgrammingCommandsType
      2.      B.3.2 Fapi_FlashBankType
      3.      B.3.3 Fapi_FlashStateCommandsType
      4.      B.3.4 Fapi_StatusType
      5.      B.3.5 Fapi_ApiProductionStatusType
    4.     B.4 结构
      1.      B.4.1 Fapi_FlashStatusWordType
      2.      B.4.2 Fapi_LibraryInfoType
  11.   C FAPI 库从 v2.00.01 到 v2.00.10 的变更摘要
  12.   D Revision History

Distribution Files

The following API files are distributed in the C2000Ware\libraries\flash_api\f280013x\folder:

  • Library Files
    • TMS320F280013x Flash API is NOT embedded into the Boot ROM of this device, it is wholly software. The software libraries provided are in EABI elf (FAPI_F280013x_EABI_v2.00.10.lib) and COFF (FAPI_F280013x_COFF_v2.00.10.lib) object formats. In order for the application to be able to erase or program the Flash/OTP, one of these two library files should be included in the application, depending on the output object format the application is using.
  • FAPI_F280013x_EABI_v2.00.10.lib – This is the Flash API EABI elf object format library (FPU32 flag enabled for build) for TMS320F280015x devices.
  • FAPI_F280013x_COFF_v2.00.10.lib – This is the Flash API COFF object format library (FPU32 flag enabled for build) for TMS320F280013x devices.
  • Fixed point version of the API library is not provided.
  • Include Files:
    • FlashTech_F280013x_C28x.h – The master include file for TMS320F280013x devices. This file sets up compile specific defines and then includes the FlashTech.h master include file.
    • hw_flash_command.h – Definitions of the flash write/erase protection registers
  • The following include files should not be included directly by the user’s code, but are listed here for user reference:
    • FlashTech.h – This include file lists all public API functions and includes all other include files.
    • Registers.h – Definitions common to all register implementations and includes the appropriate register include file for the selected device type.
    • Registers_C28x.h – Containts Little Endian and Flash memory controller registers structure.
    • Types.h – Contains all the enumerations and structures used by the API.
    • Constants/F280013x.h – Constant definitions for F280013x devices.

The following API files are distributed in the C2000Ware\libraries\flash_api\f280015x\folder:

  • Library Files
    • TMS320F280015x Flash API is NOT embedded into the Boot ROM of this device, it is wholly software. The software libraries provided are in EABI elf (FAPI_F280015x_EABI_v2.00.10.lib) and COFF (FAPI_F280015x_COFF_v2.00.10.lib) object formats. In order for the application to be able to erase or program the Flash/OTP, one of these two library files should be included in the application, depending on the output object format the application is using.
  • FAPI_F280015x_EABI_v2.00.10.lib – This is the Flash API EABI elf object format library (FPU32 flag enabled for build) for TMS320F280015x devices.
  • FAPI_F280015x_COFF_v2.00.10.lib – This is the Flash API COFF object format library (FPU32 flag enabled for build) for TMS320F280015x devices.
  • Fixed point version of the API library is not provided.
  • Include Files:
    • FlashTech_F280015x_C28x.h – The master include file for TMS320F280015x devices. This file sets up compile specific defines and then includes the FlashTech.h master include file.
    • hw_flash_command.h – Definitions of the flash write/erase protection registers
  • The following include files should not be included directly by the user’s code, but are listed here for user reference:
    • FlashTech.h – This include file lists all public API functions and includes all other include files.
    • Registers.h – Definitions common to all register implementations and includes the appropriate register include file for the selected device type.
    • Types.h – Contains all the enumerations and structures used by the API.
    • Constants/F280015x.h – Constant definitions for F280015x devices.