ZHCU831 November 2021 AWR2944 , IWR2944
The AWR2944 has the following memories:
L3 RAM for AWR2944 ES1.0: 2.25MB, ES2.0: 3MB.
Of the 32KB for L1P RAM and L1D RAM available, half (16KB) of the L1P RAM and half (16KB) of the L1D RAM are used as cache. The remaining half is reserved for code and data, and is unused.
DSS L2 RAM is used for:
DSS L3 RAM is used for:
MSS L2 RAM is used for:
Processing radar signals requires a large number of scratch buffers for each step of the processing stages. The available memory is used efficiently by overlaying the scratch buffers. A scratch buffer used in a previous stage can be re-used in the current stage. More details for this memory layout are found in the mmWave SDK documentation.