ZHCU759 July 2021
The current sense circuit is used to measure a current range over ±2 A at an accuracy range of 1%, similar to current requirements typically seen in the thermoelectric cooler. The bidirectional circuit configuration shown in Figure 2-4 converts an input current source into an output voltage. The circuit can be used on either the high side or low side of a circuit. If low-side sensing, then there are no Vcm limitations, but should not be used in applications where the system load cannot withstand small ground disturbances or in applications that need to detect load shorts. High-side sensing requires a high CMRR to reject any changes in Vbus and should not be used when common mode might exceed amplifier supply (Vcm = Vbus). For more information, see the Analog Engineer's Circuit: Low-side bidirectional current sensing circuit.
Figure 2-4 Bidirectional Current Sense
Circuit