ZHCSH09 October 2017 MSP432E401Y
PRODUCTION DATA.
Figure 4-1 shows the pinout of the 128-pin TQFP (PDT) package.
Each GPIO signal is identified by its GPIO port unless it defaults to an alternate function on reset. In this case, the GPIO port name is followed by the default alternate function. For a complete list of functions for each pin, see Table 4-2.
Figure 4-1 128-Pin PDT Package (Top View)