SWRU439M October 2015 – April 2022
There is one task code editor panel for each task code block. The Event Handler Code panels are only displayed when event trigger resources are enabled in the task panel.
To the left is the task code editor. Press F2 to open the Task Code Language Reference document in the Help Viewer (see Figure 6-7).
Figure 6-7 Task Code Editor
PanelTo the right (see Figure 6-7) are lists that show the following:
Pop-up documentation is displayed when typing the parameters and return values of a procedure. The pop-ups can also be triggered by moving the cursor to the procedure call and pressing Ctrl+Space.