SWRU439M October 2015 – April 2022
The task testing panel can be used to test a Sensor Controller task on a physical CC26xx or CC13xx device (see Figure 6-10).
Figure 6-10 Task Testing,
Setup TabDuring task testing, the Sensor Controller Studio takes over the role of the System CPU application, and it interacts with the Sensor Controller task through an XDS100, an XDS110, or an XDS200 JTAG debug probe.
The task testing panel runs whole iterations of the Initialization Code, Execution Code, Event Handler Code, and Termination Code task code blocks, and captures all task data structure values between task iterations. The data structure values are displayed graphically in the Graph tab of the task testing panel, and the values can be saved to file for external analysis.
It is also possible to automatically apply new data structure values that are loaded from file between specific task iterations.
For low-level debugging of a task, it is possible to run single iterations of the task code blocks in debug mode.