SWRA486A August   2015  – April 2017 CC1310 , CC2620 , CC2630 , CC2640 , CC2640R2F-Q1 , CC2650 , CC2650MODA

 

  1.   CC26x0, CC13x0 SimpleLink™ Wireless MCU Power Management Software Development
    1.     Trademarks
  2.   CC26x0, CC13x0 SimpleLink™ Wireless MCU Power Management Software Development
    1. 1 Abbreviations
    2. 2 Power Management Introduction
    3. 3 TI-RTOS Power Modes
      1. 3.1 Active Mode
      2. 3.2 Idle Mode
      3. 3.3 Standby Mode
        1. 3.3.1 Standby Enter Sequence
        2. 3.3.2 Standby Exit Sequence
      4. 3.4 Shutdown Mode
    4. 4 Implementation Considerations
      1. 4.1 Device Initializing
        1. 4.1.1 Low-Level Initializing
        2. 4.1.2 Initializating TI-RTOS
      2. 4.2 Recharging in Standby
      3. 4.3 Operating the DC-DC Converter
      4. 4.4 Configuring Device for External Input Interrupts and Wakeup
        1. 4.4.1 Interrupt and Wakeup from Active, Idle, and Standby
        2. 4.4.2 Wakeup from Shutdown Mode
      5. 4.5 Oscillators
        1. 4.5.1 High-Frequency Oscillators
        2. 4.5.2 Low-Frequency Oscillators
        3. 4.5.3 RC Oscillator Calibration
      6. 4.6 Auxiliary Domain
        1. 4.6.1 Powering on the Auxiliary Domain
        2. 4.6.2 Powering Down the Auxiliary Domain
        3. 4.6.3 Managing the Sensor Controller and the Auxiliary Domain Power
        4. 4.6.4 Sharing Resources Between the Sensor Controller and the Cortex®-M3
      7. 4.7 RTC
        1. 4.7.1 Initializing RTC
        2. 4.7.2 Configuring RTC Compare Events
      8. 4.8 Debugging Through Power Modes
      9. 4.9 Using Peripherals
    5. 5 References
  3.   Revision History

Using Peripherals

Peripheral drivers are part of the TI-RTOS installation. The CC26x0 and CC13x0 implementation is at the following path: C:\ti\tirtos_cc13xx_cc26xx_#_##_##_##\products\tidrivers_cc13xx_cc26xx_#_##_##_##\packages\ti\drivers

For generic peripherals such as UART, SPI, and I2C, TI-RTOS provides a common API for easy migration between different TI architectures.

The CC26x0 and CC13x0 specific drivers are documented in Doxygen format. This format explains how to use the drivers. The CC26x0 power-management document is distributed in the TI-RTOS installation. TI-RTOS Power Management User's Guide also explains how the TI-RTOS drivers interact with the power management part of the kernel.

The following rules apply when using any peripheral:

  • Only use a peripheral in active or idle power modes. In standby and shutdown, you must turn off the peripheral and its power domain.
  • Before accessing a peripheral, do the following:
    1. Turn on the power domain that contains the peripheral.
    2. Enable the run clock for the peripheral through the PRCM registers.
  • Reconfigure a peripheral before opening the input and output latches when exiting standby to avoid input and output glitches.