SWRA486A August 2015 – April 2017 CC1310 , CC2620 , CC2630 , CC2640 , CC2640R2F-Q1 , CC2650 , CC2650MODA
The Cortex-M3 must release the auxiliary force-on before entering standby and shutdown (not required when entering idle) as in Figure 20. If the sensor controller is running when AONWUCAuxWakeupEvent(...) function is called, the auxiliary domain remains on until the sensor controller idles. The system enters standby mode.
Figure 20. Powering Down the Auxiliary Domain