SWRA486A August 2015 – April 2017 CC1310 , CC2620 , CC2630 , CC2640 , CC2640R2F-Q1 , CC2650 , CC2650MODA
The CC26x0 and CC13x0 device families have an on-chip DC-DC converter which enables low-power applications. The DC-DC converter is enabled by trimDevice() based on the CCFG fields in Figure 12, and has a separate enable field for operating in active and standby modes (the hardware periodically recharges in standby mode). When the device operates in external regulator mode, disable the DC-DC converter during active and standby/recharge modes.
Figure 12. CCFG Fields For Enabling the DC-DC Converter During Active and Standby Mode Because the DC-DC converter only operates with optimum efficiency at high VDDS voltages, turn off the DC-DC converter when VDDS decreases. To configure the voltage threshold to turn off the DC-DC converter, use the CCFG field in Figure 13. Do not modify this voltage threshold.
Figure 13. The Voltage Threshold For Turning Off the DC-DC Converter The application uses the function in Figure 14, the threshold configured in the CCFG field, to decide when to turn off the DC-DC converter. The application calls this function at periodic intervals. This function also turns on the DC-DC converter if the voltage exceeds the threshold (for example, when the battery is recharging).
Figure 14. The Driverlib Function That Enables and Disables the DC-DC Converter at the Given CCFG Threshold