SPRUJ53D April 2024 ā April 2026
The ADC supports up to four sequencers, which are used to sequence the order in which ADC channels are converted. Each sequencer is associated with multiple SOCs, and the number of SOCs within a sequencer is configured using the ADCSEQ{#}CONFIG.SEQSTART and ADCSEQ{#+1}CONFIG.SEQSTART-1 or ADCSEQCTL.SEQEND registers. Sequencers are enabled using the ADCSEQ{#}CONFIG.SEQENABLE register.
Once a trigger is received for a sequencer and the ADC Wrapper is ready for arbitration, the sequencer starts converting in ascending order of SOCs. The first SOC in the sequence to convert is determined by ADCSEQ{#}CONFIG.SEQSTART, followed by subsequent SOCs until the end of the sequencer is reached.
Multiple sequencers can be configured to use the same trigger if desired. If multiple sequencers are triggered at the same time, the conversions within the sequence happens in the order of priority: SEQ1 followed by SEQ2, SEQ3, and SEQ4.
If a trigger for higher priority sequence occurs while a lower priority sequence is ongoing, the higher priority sequence can either be serviced as soon as the ongoing SOC conversion is complete or serviced after the lower priority sequence is complete. This can be configured using ADCSEQCTL.SEQPREEMPT register.
The ADCSEQCTL.SEQPREEMPT register configuration is as follows
Figure 15-4 illustrates the logical representation of sequencer{#} enable and overflow logic, which generates the overflow condition when the new trigger is received while a previous trigger is ongoing or pending.
Figure 15-5 illustrates the logical representation of sequencer{#} restart & discard logic.
Additionally, oversampling and averaging can be enabled for the SOCs within the sequence using the Post Processing Blocking (PPB) averaging feature. Each sequencer is associated with the corresponding PPB block. PPB{#}LIMIT defines the number of samples per SOCs.
If oversampling is enabled, each SOC is sampled and converted āNā times (N ā total number of samples configured) before moving to the next SOC.
Each sequencer is associated with the corresponding ADCPPB{#}TRIPHI and ADCPPB{#}TRIPLO registers. This can be used to compare whether ADCRESULT is within the configured TRIPHI and TRIPLO limits or exceeded either of the limits.
Since the limit comparator settings are common across all SOCs within a Sequencer, limit comparison for a given SOC can be enabled or disabled using the ADCSOC{#}CTL.COMPEN field of the corresponding SOC.