SPRUJ53D April 2024 – April 2026 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
If additional time between samples is desired, the application can configure SPREAD equal to the number of SYSCLK cycles desired between samples. Figure 15-12 shows an example of oversampling from an ePWM trigger with a 500-cycle spread between samples.
TRIGGER = ePWM SOCA, NSEL = 3, MODE = Oversampling, PHASE=0, SPREAD = 500
Figure 15-12 ADC Repeated Trigger Example with Sample Spread