To configure ADC oversampling or undersampling using the trigger repeater module, follow this procedure:
- Set up the SOC by writing to ADCSOCxCTL. Specify one of the two repeater modules (REP1TRIG or REP2TRIG) as the trigger source.
- Configure the repeater module by writing to the REPxCTL register:
- Configure oversampling or undersampling mode using the MODE bit.
- Specify the desired SOC trigger source in the TRIGGER field.
- If desired, configure a sync source for the repeater module in the SYNCINSEL field. A sync event resets all repeater registers to a ready and waiting state, while preserving NSEL, PHASE and MODE. A software-initiated sync is also possible by writing 1 to the SWSYNC bit.
- If desired, clear any previously set phase and trigger overflow flags by writing to the PHASEOVF and TRIGGEROVF bits.
- Configure the trigger repeat count by writing to the REPxN.NSEL register. The repeater module supports up to 128 repeats for each trigger.
- Configure the repeater phase delay by writing to the REPxPHASE.PHASE register.
- To configure a re-trigger spread delay in oversampling mode, write the desired delay value in SYSCLK cycles to the REPxSPREAD.SPREAD register.
- Configure the PPBxLIMIT register. This register defines how many samples the post-processing block accumulates before loading the partial sum value in ADCPPBxPSUM into ADCPPBxSUM.
- The post-processing block (PPB) and trigger repeater module have independent sync source configurations. To configure the PPB sync source, write to the ADCPPBxCONFIG2 register. For more information on how to configure the ADC post-processing block, see Section 15.8.
Note: When NSEL = 0, the repeater module essentially acts as a pass-through for SOC triggers, but is still useful for applying phase delay. SOC triggers are passed through
in both oversampling and undersampling mode, even if there are still pending SOCs. In this scenario, the ADC sets a trigger overflow flag for the individual SOC (ADCSOCOVF1.SOCx), not the repeater module. When oversampling with NSEL > 0, the ADC sets the oversampled trigger overflow flag
(REPxCTL.TRIGGEROVF) if a trigger arrives while there are pending SOCs.
When NSEL = 0, the repeater module does not set the REPxCTL.MODULEBUSY indicator. In this scenario, the application must make sure that all associated SOC flags have completed before enabling oversampling or undersamplingmode by setting NSEL > 0.
Table 15-4 ADC SYNC Input
| ADCPPBxCONFIG2. SYNCINSEL |
Connection from |
| 0 |
Disable SyncIn to PPBx |
| 1 |
EPWM1_SYNCOUT |
| 2 |
EPWM2_SYNCOUT |
| 3 |
EPWM3_SYNCOUT |
| 4 |
EPWM4_SYNCOUT |
| 5 |
EPWM5_SYNCOUT |
| 6 |
EPWM6_SYNCOUT |
| 7 |
EPWM7_SYNCOUT |
| 8 |
EPWM8_SYNCOUT |
| 9 |
EPWM9_SYNCOUT |
| 10 |
EPWM10_SYNCOUT |
| 11 |
EPWM11_SYNCOUT |
| 12 |
EPWM12_SYNCOUT |
| ... |
N/A |
| 19 |
ECAP1_SYNCOUT |
| 20 |
ECAP2_SYNCOUT |
| ... |
N/A |
| 26 |
INPUTXBAR5 |
| 27 |
INPUTXBAR6 |
| ... |
N/A |
| 31 |
N/A |