SPRUIU8B August   2020  – March 2026 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1

 

  1.   1
  2.   Live Firmware Update With Device Reset on C2000 MCUs
  3.   Trademarks
  4. 1Introduction
  5. 2Resources Required for LFU
  6. 3Memory Layout
  7. 4Static Code in LFU
  8. 5LED Example Application and LFU Flow
  9. 6Running the LED Example
    1. 6.1 Serial Flash Programmer Update
    2. 6.2 Programming Static Code – Loading via Code Composer Studio (CCS)
    3. 6.3 Live Firmware Update of Application
    4. 6.4 Limitations and Troubleshooting
  10. 7Extended Implementations
    1. 7.1 Live Firmware Update with Reset on F28P65x MCUs
      1. 7.1.1 F28P65x LFU Hardware Requirements
      2. 7.1.2 Flash Organization
      3. 7.1.3 FWU Boot Mode
      4. 7.1.4 LED Example Application
        1. 7.1.4.1 LFU Command Processing
      5. 7.1.5 Running the Example
        1. 7.1.5.1 Loading the Example
        2. 7.1.5.2 Combing CPU1 and CPU2 Firmware Images
        3. 7.1.5.3 LFU over MCAN Host Programmer
          1. 7.1.5.3.1 Compiling the Host Programmer
          2. 7.1.5.3.2 Using the Host Programmer
      6. 7.1.6 Restrictions
  11. 8Revision History

Resources Required for LFU

LFU is feasible when the device has enough resources of various kinds – CPU bandwidth, Memory, and Peripheral availability:

  • CPU Bandwidth – The new firmware has to be transferred using a communication peripheral and written to flash memory while the application is still operating. This means CPU need to have enough available bandwidth to support LFU.
  • Memory – The non-volatile memory that is used here is Flash memory. Flash read and write operations cannot be simultaneously performed on the same Flash bank. However read and write operations can be simultaneously performed on different Flash banks. Hence, the ideal scenario is for the device to contain dual Flash banks. In devices with single Flash banks, LFU is particularly challenging, but still feasible provided:
    • The complete application code (or a portion of it that controls the output(s) the user is interested in) and Flash APIs need to run from RAM memory while the new firmware is updated to Flash. This means there should be enough RAM memory that can be utilized.
    • Some devices support Flash APIs in ROM; in those devices the application code can run from RAM and Flash APIs can run from ROM memory, thus reducing the RAM requirement.
  • Peripheral Availability – A spare communication peripheral using the new image can be transferred from the host to the device.

LFU is easier to implement in devices with multiple Flash banks. In this document and the reference example, it is assumed that the device has 2 Flash banks. The device considered is TMS320F28004x, which has dual flash banks. Their address space is 64K x 16 each, with addresses ranging from 0x80000-0x8FFFF, and 0x90000-0x9FFFF.