SPRUIU8B August 2020 – March 2026 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
The hardware used in the illustrated steps is an F28004x ControlCARD on a ControlCARD docking station Rev4.1. If a JTAG connection is available, then CCS can be used to load Flash banks 0 and 1 with static code. Note:
Make sure you have the settings in CCS (or your target configuration file – by right clicking and selecting properties) as shown in Figure 6-1 before loading the images. Build the flashapi_ex2_sci_kernel project in both BANK0_LDFU and BANK1_LDFU configurations, and load each to target. The CCS flash plugin will load the contents on to flash.
Figure 6-1 Flash Settings to Only Erase Necessary Sectors
Figure 6-2 Selecting Kernel to Load to Flash Bank 0After the static contents are loaded on BANK0, the first thing that happens is the execution of the bank selection logic that will determine that application firmware is not programmed in either bank.
Control will pass to the flash kernel, which will be ready to program the application in BANK1. The CCS view will look Figure 6-3 (the program will not stop at main(), but will be running, awaiting a SCI command):
Figure 6-3 CCS Window view After Programming Bank 0 Flash Kernel
Figure 6-4 CCS Memory Browser View to Verify Successful Kernel Programming of Bank 0
Figure 6-5 LFU Serial Command Invoked From Windows Command Prompt
Figure 6-6 Successful Completion of LFU Command to Program Flash Bank 1
Figure 6-7 CCS Memory Browser View to Verify Successful Programming of Application on Bank 1The kernel will also update the KEY and revision number in BANK1 sector 2. Now the static image, in programmed BANK0 and application image, is programmed in BANK1.
Figure 6-8 Selecting Kernel to Load to Flash Bank 1
Figure 6-9 CCS Memory Browser View to Verify Successful Kernel Programming of Bank 1After the static contents are loaded on to BANK1, execution stops at main(). This occurs for the kernel on Bank1 because bank selection logic resides only on Bank0, not on Bank1. Thus, for Bank1, execution flow follows the conventional flow of codestart leading up to main().
Figure 6-10 CCS Window View After Programming Bank 1 Flash Kernelserial_flash_programmer_appln.exe -d f28004x -k f28004x_fw_upgrade_example\flashapi_ex2_sci_kernel.txt -a flashapi_ex3_live_firmware_updateBANK0FLASH.txt -b 9600 -p COMx where x = COM port corresponding to the JTAG connection between the PC and the target board. flashapi_ex3_live_firmware_updateBANK0FLASH.txt is generated by building the CCS project flashapi_ex3_live_firmware_update in build configuration BANK0_FLASH.
Figure 6-11 LFU Serial Command Invoked From Windows Command Prompt
Figure 6-12 Successful Completion of LFU Command to Program Flash Bank 0The kernel will also update the KEY and revision number in BANK0 sector 2. Now the static image in programmed BANK1 and application image is programmed in BANK0.