SPRU513Y August 2001 – June 2022 SM320F28335-EP
The SECTIONS directive is specified in a command file by the word SECTIONS (uppercase), followed by a list of output section specifications enclosed in braces.
The general syntax for the SECTIONS directive is:
| SECTIONS | |
| { | |
| name : [property [, property] [, property] . . . ] | |
| name : [property [, property] [, property] . . . ] | |
| name : [property [, property] [, property] . . . ] | |
| } | |
Each section specification, beginning with name, defines an output section. (An output section is a section in the output file.) Section names can refer to sections, subsections, or archive library members. (See Section 9.6.5.4 for information on multi-level subsections.) After the section name is a list of properties that define the section's contents and how the section is allocated. The properties can be separated by optional commas. Possible properties for a section are as follows:
|
|||
| Syntax: | load = allocation | or | |
| > allocation | |||
|
|||
| Syntax: | run = allocation | or | |
| run > allocation | |||
|
|||
| Syntax: | { input_sections } | ||
|
|||
| Syntax: | type = COPY | or | |
| type = DSECT | or | ||
| type = NOLOAD | |||
|
|||
| Syntax: | fill = value | ||
The SECTIONS Directive shows a SECTIONS directive in a sample linker command file. (This example uses COFF section names.)
/**************************************************/
/* Sample command file with SECTIONS directive */
/**************************************************/
file1.c.obj file2.c.obj /* Input files */
--output_file=prog.out /* Options */
SECTIONS
{
.text: load = PROG, PAGE = 0,
run = 0x0200, PAGE = 1
.econst: load = RAM1
.ebss: load = RAM1
.scratch: load = 0x0060, PAGE = 1
{
t1.c.obj(.scratch1)
t2.c.obj(.scratch2)
endscratch = .;
}
.data:alpha: align = 16
.data:beta: align = 16
}Figure 9-3 shows the output sections defined by the SECTIONS directive in The SECTIONS Directive (.vectors, .text, .econst, .ebss, .data:alpha, and .data:beta) and shows how these sections are allocated in memory using the MEMORY directive given in The MEMORY Directive.
Figure 8-3 Section
Placement Defined by The SECTIONS Directive