SPRU513Y August 2001 – June 2022 SM320F28335-EP
The C/C++ compiler uses an uninitialized section called .esysmem for the C run-time memory pool used by malloc(). You can set the size of this memory pool at link time by using the --heap_size option. The syntax for the --heap_size option is:
--heap_size= size
The size must be a constant. This example defines a 4K word heap:
cl2000 --run_linker --heap_size=0x1000 /* defines a 4k heap (.esysmem section)*/The linker creates the .esysmem section only if there is a .esysmem section in an input file.
The linker also creates a global symbol, __SYSMEM_SIZE (for COFF) or __TI_SYSMEM_SIZE (for EABI), and assigns it a value equal to the size of the heap. The default size is 1K words. See Section 9.7.1 for information about referring to linker symbols in C/C++ code. For more about C/C++ linking, see Section 9.12.