SPRU513Y August 2001 – June 2022 SM320F28335-EP
For the COFF ABI, the linker automatically defines symbols for those sections used in your assembly source. A program can use these symbols at run time to determine where a section is linked. Since these symbols are external, they appear in the linker map. You must have used the corresponding section in a source module for the symbol to be created. Values are assigned to these symbols as follows:
| .text | is assigned the first address of the .text output section. (It marks the beginning of executable code.) | |
| etext | is assigned the first address following the .text output section. (It marks the end of executable code.) | |
| .data | is assigned the first address of the .data output section. (It marks the beginning of initialized data tables.) | |
| edata | is assigned the first address following the .data output section. (It marks the end of initialized data tables.) | |
| .ebss | is assigned the first address of the .ebss output section. (It marks the beginning of uninitialized data.) | |
| end | is assigned the first address following the .ebss output section. (It marks the end of uninitialized data.) |
The linker automatically defines the following symbols for C/C++ support when the --ram_model or --rom_model option is used.
| __TI_STACK_SIZE | is assigned the size of the .stack section. (EABI) | |
| __TI_STACK_END | is assigned the end of the .stack section. (EABI) | |
| __TI_SYSMEM_SIZE | is assigned the size of the .sysmem section. (EABI) | |
| __STACK_SIZE | is assigned the size of the .stack section. (COFF) | |
| __STACK_END | is assigned the end of the .stack section. (COFF) | |
| __SYSMEM_SIZE | is assigned the size of the .esysmem section. (COFF) |
These linker-defined symbols can be accessed in any assembly language module if they are declared with a .global directive (see Identify Global Symbols).
See Section 9.7.1 for information about referring to linker symbols in C/C++ code.