SPRADQ4 December   2025 AM2612 , AM2631 , AM2632 , AM2634 , AM263P2 , AM263P4

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Hardware and Software Preparation
  6. 3How to Generate the ETHERCAT Stack Code for AM263P
  7. 4How to Run the AM263 EVM with the ETHERCAT
  8. 5How to Run the TwinCAT
  9. 6Demo
  10. 7References

How to Run the TwinCAT

This tool is to test your ETHERCAT code on the AM263.

The Topology is this:

PC / NB → Run with TwinCAT ← Ethernet → AM263 with ETHERCAT.

The user must read these important documents first:

Follow these steps:

  1. Install this package; it must match your Windows version:

    https://cstweb.wtb.tue.nl/4tc00/_downloads/d67baccd94aeeeb468136e6aad54629a/TC31-Full-Setup.3.1.4024.56.exe

  2. Go to your Windows Networking setting, choose the Ethernet1 (the Default port.)
  3. Check the “TwinCAT RT-Ethernet Filter Driver”, as shown here:
     TWINCAT Driver in the Network Setting Figure 5-1 TWINCAT Driver in the Network Setting
  4. Install the TWINCAT.
     Installed the TWINCAT Driver Completed Figure 5-2 Installed the TWINCAT Driver Completed
  5. Go to the device manager, check “Network adapters”, and check if this one is present: TwinCAT Intel PCI Ethernet Adapter (Gigabit), as in the following:
     TWINCAT Intel Driver
                            Installed in the DevMgr Figure 5-3 TWINCAT Intel Driver Installed in the DevMgr
  6. Launch the TWINCAT XAE.
  7. Go to “Device”, Click “Scan”, as in following:
     Scan the Box Figure 5-4 Scan the Box
  8. This “Activate Free Run” is a mandatory key step, without this box showing, the TwinCAT will not work.
     Activate Free Run Example Figure 5-5 Activate Free Run Example