SPRADQ4 December   2025 AM2611 , AM2612 , AM2612-Q1 , AM2631 , AM2632 , AM2634 , AM263P2 , AM263P4

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Hardware and Software Preparation
  6. 3How to Generate the ETHERCAT Stack Code for AM263P
  7. 4How to Run the AM263 EVM with the ETHERCAT
  8. 5How to Run the TwinCAT
  9. 6Demo
  10. 7References

How to Run the AM263 EVM with the ETHERCAT

Follow these steps:

  1. Set the SW5 on the EVM to use XDS110 JTAG, as in the following image:
     EVM SW5 Switch – XDS110 Figure 4-1 EVM SW5 Switch – XDS110
  2. Connect to the PRU0 port. This port is the default one to test the ETHERCAT, as in the following image:
     Default PRU0 ETHERCAT Tested Port Figure 4-2 Default PRU0 ETHERCAT Tested Port
  3. Create the AM263.ccxml, set as XDS110, and test the JTAG first.
  4. Launch the AM263.ccxml.
  5. Connect to the R5F_0 core, as in the following image:
     R5F_Core 0 Position Figure 4-3 R5F_Core 0 Position
  6. Download the ETHERCAT built code, as in the following image:
     R5F_Core 0 Selected Figure 4-4 R5F_Core 0 Selected
  7. Free run the code, and open your teraterm console log; you will see the following screen.
     ETHERCAT Running Console Log Example Figure 4-5 ETHERCAT Running Console Log Example