SPRADQ4 December 2025 AM2612 , AM2631 , AM2632 , AM2634 , AM263P2 , AM263P4
Read this Readme file in the SDK path: C:\ti\ind_comms_sdk_am263x_09_02_00_13\source\industrial_comms\EtherCAT_slave\beckhoff_stack\stack_sources
There are two ways to generate the ETHERCAT Salve Stack code.
TI recommends using the first option (Using the patch file) to generate the code, as the user does not need to find and learn the Beckoff SSC Tool.
Follow these steps:
patch.exe
-i C:\TI\ind_comms_sdk_am263x_09_02_00_13/source/industrial_comms/EtherCAT_slave/beckhoff_stack/patch/TI_ETHERCAT.patch
-d C:\TI\ind_comms_sdk_am263x_09_02_00_13/source/industrial_comms/EtherCAT_slave/beckhoff_stack/stack_sources/
When you perform the patch.exe, you can manually assign the file path + file name together. as shown here:
Figure 3-1 SSC Patch
Example
Figure 3-2 ETHERCAT Code
Build-out