SPMU378 April 2026 TPS26750A
In this document the register names use an ALL CAPS notation, and the field names use a CamelBack notation. For example TX_SOURCE_CAPS refers to register 0x32, and TX_SOURCE_CAPS.numValidPDOs refers to a specific field in Byte 1 of that register.
Some registers have the same definition, but there are multiple instantiations at different register addresses. The following lists these registers.
In this document, the "x" indicates that it is referring to both instantiations of that register.