SPMU378 April   2026 TPS26750A

 

  1.   1
  2.   Read This First
    1.     About This Manual
    2.     Notational Conventions
    3.     Glossary
    4.     Related Documents
    5.     Support Resources
    6.     Trademarks
  3. 1Introduction
    1. 1.1 Introduction
      1. 1.1.1 Purpose and Scope
    2. 1.2 PD Controller Host Interface Description
      1. 1.2.1 Overview
      2. 1.2.2 Register and field notation
    3. 1.3 Unique Address Interface
      1. 1.3.1 Unique Address Interface Protocol
  4. 2PD Controller Policy Modes
    1. 2.1 Overview
    2. 2.2 Source Policy Mode
    3. 2.3 Sink Policy Mode
  5. 3Register Overview
    1. 3.1 TPS26750A Registers
  6. 44CC Task Detailed Descriptions
    1. 4.1 Overview
    2. 4.2 CPU Control Tasks
      1. 4.2.1 'Gaid' - Return to normal operation
      2. 4.2.2 'GAID' - Cold reset request
    3. 4.3 PD Message Tasks
      1. 4.3.1  'SWSk' - PD PR_Swap to Sink
      2. 4.3.2  'SWSr' - PD PR_Swap to Source
      3. 4.3.3  'SWDF' - PD DR_Swap to DFP
      4. 4.3.4  'SWUF' - PD DR_Swap to UFP
      5. 4.3.5  'GSkC' - PD Get Sink Capabilities
      6. 4.3.6  'GSrC' - PD Get Source Capabilities
      7. 4.3.7  'ESkC' - PD EPR Get Sink Capabilities
      8. 4.3.8  'ESrC' - PD EPR Get Source Capabilities
      9. 4.3.9  'SSrC' - PD Send Source Capabilities
      10. 4.3.10 'GPPI' - PD Get Port Partner Information
      11. 4.3.11 'MBRd' - Message Buffer Read
    4. 4.4 Patch Bundle Update Tasks
      1. 4.4.1  'PBMs' - Start Patch Burst Mode Download Sequence
      2. 4.4.2  'PBMc' - Patch Burst Mode Download Complete
      3. 4.4.3  'PBMe' - End Patch Burst Mode Download Sequence
      4. 4.4.4  'GO2P' - Go to Patch Mode
      5. 4.4.5  'PTCs' - Start Patch Download Sequence
      6. 4.4.6  'PTCd' - Patch Download
      7. 4.4.7  'PTCc' - Patch Download Complete
      8. 4.4.8  'PTCq' - Patch Query
      9. 4.4.9  'PTCr' - Patch Reset
      10. 4.4.10 'FLrd' - Flash Memory Read
      11. 4.4.11 'FLad' - Flash Memory Write Start Address
      12. 4.4.12 'FLwd' - Flash Memory Write
      13. 4.4.13 'FLvy' - Flash Memory Verify
    5. 4.5 System Tasks
      1. 4.5.1 'ANeg' - Auto Negotiate Sink Update
      2. 4.5.2 'DBfg' - Clear Dead Battery Flag
      3. 4.5.3 'I2Cr' - I2C read transaction
      4. 4.5.4 'I2Cw' - I2C write transaction
      5. 4.5.5 'GPsh' - set GPIO high
      6. 4.5.6 'GPsl' - set GPIO low
  7. 5User Reference
    1. 5.1 PD Controller Application Customization
    2. 5.2 Loading a Patch Bundle
    3. 5.3 AUTO_NEGOTIATE_SINK Register
      1. 5.3.1 AUTO_NEGOTIATE_SINK Usage Example 1
      2. 5.3.2 AUTO_NEGOTIATE_SINK Usage Example 2
      3. 5.3.3 AUTO_NEGOTIATE_SINK Usage Example 3
      4. 5.3.4 AUTO_NEGOTIATE_SINK Usage Example 4
    4. 5.4 Liquid Detection Registers
    5. 5.5 GPIO Events
  8. 6Revision History

Overview

This section describes the 4CC Tasks defined by the PD Controller Host Interface. The Tasks are categorized into various sub-groups in this section. All Tasks that return data using the DATAx registers will always ensure the proper output data is loaded into those registers before setting the CMDx register to 0 to indicate Task completion. DATAx is never modified by PD Controller after CMDx has been changed to 0, to ensure the Host can retrieve data from the previously-executed Task, and to ensure the Host can load these registers for a future Task without risk of overwriting. Note that other registers can continue to be updated after a Task completes, as Tasks can have additional side effects.

Many of the Tasks return a status code in the first byte of the DATAx register. The standard Task response byte is defined in Table 4-1. The remaining DATAx bytes can be used at each Task's discretion.

Table 4-1 Standard Task Response
DescriptionTasks are a special form of Tasks that return a status code in the first byte of the DATAX register.
Output DATAXBitNameDescription
Byte 1: Task Return Code
7:4ReservedReserved for standard Tasks. May be used by certain Tasks for Task-specific return codes. Successful return codes can use this byte provided TaskResult is 0x0.
3:0TaskResultStandard Task return codes.
0x0Task completed successfully.
0x1Task timed-out.
0x2Reserved.
0x3Task rejected.
0x4Task rejected because the Rx Buffer was locked. This is for Tasks that can require the PD controller to use the Rx Buffer.
0x5-0xFReserved for standard Tasks. May be used by certain Tasks for Task-specific error codes. Treated as an error when encountered.