SNVU944 March 2026 TPS7H1301-SP
Calculate the expected VDroop and VDropout requirements for the expected load when selecting VIN and VOUT.
Ensure proper orientation of components on the negative rails (such as tantalum capacitors).
Determine VIN ripple requirements when selecting input capacitance.
Be aware of areas of the board that may heat up during operation.
![]() |
| Hot surface. Contact can cause burns. Do Not Touch! |