SNAU260A October 2020 – February 2021
ADVANCE INFORMATION
The Input Page provides a high level view of all the inputs for the device, the APLL frequency, and DPLL frequency of the device.
Figure 6-8 Inputs LocationOnce the DPLL dividers and loop filter have been calculated by running the script in step 7 on the start page, this page displays the DPLL divider values which set the DPLL frequency. Here it is shown that the DPLL frequency is the exact desired frequency.
Each DPLL supports two sets of DPLL dividers which can be selected. At this time, the tool calculates the divider for FB Config 1 only. Div #1 settings may be copied into Div #2 settings and selected for use by the DPLL Div Select control.
On this page, it is possible to select the APLL frequency or DPLL frequency to propagate through to the outputs by changing APLL frequency to DPLL frequency.
Figure 6-9 APLL or DPLL Frequency
Selection
Figure 6-10 PLL3 Input