SLVUB95C December   2017  – August 2018

 

  1.   DRV10974 Evaluation Module
    1.     Trademarks
    2. DRV10974 EVM Kit Contents
    3. Introduction
      1. 2.1 Features
    4. Quick Start Guide
    5. DRV10974 Onboard Connections
      1. 4.1 Connector (P1) for Power Input
      2. 4.2 Interface Connector (P2) for Phase Windings of Motor
    6. DRV10974 Package
    7. User Interface
      1. 6.1 Jumpers
      2. 6.2 Switch
      3. 6.3 Test Points
    8. CS, RMP, and ADV Resistor Selection
      1. 7.1 CS Resistor Table
      2. 7.2 RMP Resistor Table
      3. 7.3 ADV Resistor Table
    9. Schematic
    10. Bill of Materials (BOM)
    11. 10 EVM Documentation
  2.   Revision History

Jumpers

Descriptions for the jumpers are provided in the following list:

cs-receptable-j10.gifFigure 8. CS Receptacle (J10)
  • CS (J10) is the current limit setting. CS connects a resistor to GND for current-limit setting. This receptacle is meant for easy implementation of axial-lead through-hole resistors. Otherwise, R4 can be used for substitution of surface-mount resistors.
  • adv-receptable-j8.gifFigure 9. ADV Receptacle (J8)
  • ADV (J8) is the lead angle setting. ADV connects a resistor to GND for lead angle setting. This receptacle is meant for easy implementation of axial-lead through-hole resistors. Otherwise, R2 can be used for substitution of surface-mount resistors.
  • rmp-receptacle-j9.gifFigure 10. RMP Receptacle (J9)
  • RMP (J9) is the acceleration ramp-rate control setting. RMP connects a resistor to GND for setting the acceleration ramp-rate control. This receptacle is meant for easy implementation of axial-lead through-hole resistors. Otherwise, R3 can be used for substitution of surface-mount resistors.
  • speed-command-input-select-header-j3.gifFigure 11. Speed Command Input Select Header (J3)
  • Select (J3) is used to configure motor speed-control resources for the PWM pin. Set the PWM jumper to PWMIN for sending a PWM signal to the PWM pin to control motor speed. See Figure 4 for more details. Set the PWM jumper to Analog with J2 connected for using potentiometer (R5) to control motor speed. See Figure 3 for more details.
  • J7 and J11 Connections are placeholders for an I2C interface, so they can be ignored.
  • potentiometer-power-header-j2.gifFigure 12. Potentiometer Power Header (J2)
  • Potentiometer Power (J2) provides voltage from the V1P8 pin of the DRV10974 device to power the potentiometer. This header must be jumpered to use the potentiometer.