SLVK326 May 2026 ADS1278QML-SP
The purpose of this study was to characterize the effect of heavy-ion irradiation on the single-event effect (SEE) performance of the ADS1278QML-SP 24-bit, delta-sigma analog-to-digital converter (ADC). Heavy-ions with LETEFF = 51 MeV×cm2/mg were used for the SEE characterization campaign. Flux of ≈104 to 105 ions/cm2 ×s and fluences of ≈106 to 107 ions/cm2 per run were used for the characterization. The SEE results demonstrated that the ADS1278QML-SP is free of destructive SEL at LETEFF = 51 MeV×cm2/mg and across the full electrical specifications.