SLVK227 October   2025 TPS7H4012-SP , TPS7H4013-SP

 

  1.   1
  2.   TPS7H4012-SP and TPS7H4013-SP Single-Event Effects (SEE)
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Depth, Range, and LETEFF Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
  12. 9 Event Rate Calculations
  13. 10Summary
  14.   A References

Single-Event Latch-up (SEL) Results

During the SEL testing the device was heated to 125°C by using a Closed-Loop PID controlled heat gun (MISTRAL 6 System (120V, 2400W)). The temperature of the die was constantly monitored during testing at TAMU through an IR camera integrated into the control loop to create closed-loop temperature control.

The species used for the SEL testing was Holmium (165Ho at 15MeV/nucleon). For the 165Ho ion an incidence angle of 0° was used to achieve an LETEFF = 75 MeV×cm2/mg (For more details, see Table 5-1). The kinetic energy in the vacuum for this ions is 2.474 GeV. Flux of ≈1 × 105 ions/cm2/s and a fluence of ≈107 ions/cm2 per run was used. Run duration to achieve this fluence was ≈2 minutes. The eight devices were powered up and exposed to the heavy-ions using the maximum recommended input voltage of 14V with the maximum recommended load of each respective device. No SEL events were observed during all eight runs, indicating that the TPS7H401x-SP is SEL-free up to 75 MeV×cm2/mg. Note that due to the performance of the TPS7H4011-SP an experiment was conducted with the TPS7H4012-SP and the TPS7H4013-SP to determine if a SW to GND Schottky diode was required for operation during SEE testing. As shown in the table below it was found that both the TPS7H4012-SP and TPS7H4013-SP pass the full SEL run conditions regardless of whether or not the Schottky is present, indicating the Schottky is not required for SEE performance.Table 8-4 shows the SEL test conditions and results. Figure 7-1 shows a plot of the current versus time for run 3.

Table 7-1 Summary of TPS7H401x-SP SEL Test Condition and Results

Device

Run NumberUnit Number

SW to GND Schottky?

IonLETEFF (MeV × cm2/mg)Flux (ions/cm2/s)Fluence (ions /cm2)VINIOUT (A)SEL (# Events)

TPS7H4012-SP

11

Yes

165Ho759.76 × 1041 x 10714

6

0
22

Yes

165Ho759.72 × 1041 x 10714

6

0
33

No

165Ho751.08 × 1051 x 10714

6

0
44

No

165Ho751.02 × 1051 × 10714

6

0

TPS7H4013-SP

5

5

Yes165Ho751.07 × 1051 × 10714

3

0

6

6

Yes165Ho751.09 × 1051 × 10714

3

0

7

7

No165Ho751.26 × 1051 × 10714

3

0

8

8

No165Ho751.28 × 1051 × 10714

3

0

Using the MFTF method shown in Single-Event Effects (SEE) Confidence Interval Calculations and combining (or summing) the fluences of the eight runs at 125°C (8 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated as: σSEL ≤ 4.61 × 10-8 cm2/device for LETEFF = 75 MeV×cm2/mg and T = 125°C.
 SEL Current versus Time for Run 3 of the TPS7H4013-SP at T = 125°C (VOUT = 3.3V)Figure 7-1 SEL Current versus Time for Run 3 of the TPS7H4013-SP at T = 125°C (VOUT = 3.3V)