SLVK227 October   2025 TPS7H4012-SP , TPS7H4013-SP

 

  1.   1
  2.   TPS7H4012-SP and TPS7H4013-SP Single-Event Effects (SEE)
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
  7. 4 Irradiation Facility and Setup
  8. 5 Depth, Range, and LETEFF Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
  12. 9 Event Rate Calculations
  13. 10Summary
  14.   A References

Test Setup and Procedures

There were two input supplies used to power the TPS7H401x-SP which provided VIN and EN. The VIN for the device was provided through Channel 3 of an N6705C power module and ranged from 5 and 12V for SET to 14V for SEL and SEB/SEGR. EN was powered by Channel 1 of an E36311A power supply and ranged from 0V for SEB Off to 5V for all other testing. AUX_5V was supplied via channel 2 of an E36311A power supply in order to drive PWRGD high to 5V during the SEE testing.

The instrument used to load the TPS7H401x-SP was a Chroma 63600 E-Load that was used in Constant Resistance (CR) mode. For the TPS7H4012-SP, the value of CR was 0.5436Ω and provided a 6A load on the device. For the TPS7H4013-SP, the value of CR was 1.0872Ω and provided a 3A load on the device.

The primary signal monitored on the EVM was VOUT and this was done using a PXIe-5172 scope card with a 3% window trigger based on the nominal measured value of VOUT. All SEL, SEB On, and SET testing used these conditions with only the SEB Off testing having different conditions. The conditions for SEB Off were a positive edge trigger at 0.5V which would check to see if the device ever incorrectly turned on while it was disabled. The secondary signals monitored were the PWRGD and SS_TR pins. These signals were monitored on their own PXIe-5172 cards and were configured to have negative edge triggers. Both had a negative edge trigger at 50% below nominal.

All equipment was controlled and monitored using a custom-developed LabVIEW™ program (PXI-RadTest) running on a HP-Z4™ desktop computer. The computer communicates with the PXI chassis via an MXI controller and NI PXIe-8381 remote control module.

Table 6-1 shows the connections, limits, and compliance values used during the testing. Figure 6-1 shows a block diagram of the setup used for SEE testing of the TPS7H4012-SP and Figure 6-2 shows a block diagram of the setup used for SEE testing of the TPS7H4013-SP.

Table 6-1 Equipment Settings and Parameters Used During the SEE Testing of the TPS7H401x-SP
Pin NameEquipment UsedCapabilityComplianceRange of Values Used
VINN6705C (CH #3)60V, 17A5A5 to 14V
ENE36311A (CH #1)6V, 5A0.1A0V, 5V

AUX_5V

E36311A (CH #2)

25V, 1A

0.1A

5V

VOUTPXIe-5172 (1)100MS/s—100MS/s
SS_TRPXIe-5172 (2)100MS/s—100MS/s
PWRGDPXIe-5172 (3)100MS/s—100MS/s
VOUTChroma 63600 E-Load80AHigh—

All boards used for SEE testing were fully checked for functionality. Dry runs were also performed to ensure that the test system was stable under all bias and load conditions prior to being taken to the test facilities. During the heavy-ion testing, the LabVIEW control program powered up the TPS7H401x-SP device and set the external sourcing and monitoring functions of the external equipment. After functionality and stability was confirmed, the beam shutter was opened to expose the device to the heavy-ion beam. The shutter remained open until the target fluence was achieved (determined by external detectors and counters). During irradiation, the NI scope cards continuously monitored the signals. When the output exceeded the pre-defined 3% window trigger, a data capture was initiated. No sudden increases in current were observed (outside of normal fluctuations) on any of the test runs and indicated that no SEL or SEB/SEGR events occurred during any of the tests.

 Block Diagram of the SEE Test Setup for the TPS7H4012-SPFigure 6-1 Block Diagram of the SEE Test Setup for the TPS7H4012-SP
 Block Diagram of the SEE Test Setup for the TPS7H4013-SPFigure 6-2 Block Diagram of the SEE Test Setup for the TPS7H4013-SP