SLUUBW5A July 2018 – September 2021 BQ34Z100-G1
Texas Instruments ships the BQ34Z100-G1 device in I2C mode, which is required when updating data flash. However, this mode can be changed to HDQ mode if needed.
To configure the device to use I2C mode when presently in the HDQ mode, a write to the Control command [0x00] of [0x29E7] is required. Use the Battery Management Studio (BQSTUDIO) tool, as follows: