SLUAAB9A March 2021 – December 2021 UCC25800-Q1
Besides the transformer turns-ratio, the LLC converter voltage gain is also affected by the rectification structure. In this section, a few rectification methods are presented and designers can select the one according to their cost structure from the components. Because the primary-side circuit remains the same, the description only focuses on the secondary-side circuit.