SLAU780 August 2018
The SimpleLink MSP432E4 Software Development Kit (SDK) provides drivers for all of the peripheral devices supplied in the design. The Peripheral Driver Library is required to operate the on-chip peripherals as part of the SDK. The SDK includes a set of example applications that use the Peripheral Driver Library. These applications demonstrate the capabilities of the MSP432E411Y microcontroller and provide a starting point for the development of the final application for use on the MSP432E411Y-BGAEVM.