SFFS983A August 2025 – October 2026 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0G3529-Q1
In this method, an incorrect ECC value (for the corresponding data) is written and a read from the same location is performed. The test checks that an ECC error occurs (single or double-bit error, depending on how many bits were corrupted). Using unchecked memory aperture, data bits can be written independent of ECC bits. When the same location is accessed from the region which was checked through ECC, an ECC error occurs. This method can be used to check the ECC logic.