SDAA260 April   2026 CC1310 , CC1311P3 , CC1312PSIP , CC1312R , CC1312R7 , CC1314R10 , CC1350 , CC1352P , CC1352P7 , CC1352R , CC1354P10 , CC1354R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2PHY Settings Exported with the Standard Commands
    1. 2.1 Standard Packet Format (1 Length Byte)
      1. 2.1.1 TX using CMD_PROP_TX and Standard Packet Format (1 Length Byte)
      2. 2.1.2 RX using CMD_PROP_RX and Standard Packet Format (1 Length Byte)
      3. 2.1.3 TX using CMD_PROP_TX_ADV and Standard Packet Format (1 Length Byte)
      4. 2.1.4 RX using CMD_PROP_RX_ADV and Standard Packet Format (1 Length Byte)
    2. 2.2 Standard Packet Format (2 Length Bytes)
      1. 2.2.1 TX using CMD_PROP_TX_ADV and Standard Packet Format (2 Length Bytes)
      2. 2.2.2 RX Using CMD_PROP_RX_ADV and Standard Packet Format (2 Length Bytes)
  6. 3TX and RX Settings Exported with the Advanced Commands
    1. 3.1 Advanced Packet Format
      1. 3.1.1 TX using CMD_PROP_TX_ADV and Advanced Packet Format
      2. 3.1.2 RX using CMD_PROP_RX_ADV and Advanced Packet Format
    2. 3.2 Standard Packet Format (1 Length Byte)
      1. 3.2.1 TX using CMD_PROP_TX_ADV and Standard Packet Format (1 Length Byte)
      2. 3.2.2 RX using CMD_PROP_RX_ADV and Standard Packet Format (1 Length Byte)
    3. 3.3 Standard Packet Format (2 Length Bytes)
      1. 3.3.1 TX using CMD_PROP_TX_ADV and Standard Packet Format (2 Length Bytes)
      2. 3.3.2 RX using CMD_PROP_RX_ADV and Standard Packet Format (2 Length Bytes)
  7. 4References

TX using CMD_PROP_TX_ADV and Standard Packet Format (1 Length Byte)

In some cases, the user would want to use the advanced command to transmit a packet, even if the packet format is the standard one. This could be because they eventually want to transmit a longer preamble than what is supported by the standard TX command, for example in a Sniff Mode application.

Both SysConfig (3) and SmartRF Studio (2) support importing and exporting other commands than what is used for a PHY by default. Figure 2-2 shows how to select extra commands to be imported to a project using SysConfig, and Figure 2-3 shows how this is done with code exports using SmartRF Studio.

 Importing the Advanced TX
                    Command in addition to the Standard Command in SysConfig Figure 2-2 Importing the Advanced TX Command in addition to the Standard Command in SysConfig
 Exporting the Advanced TX
                    Command in addition to the Standard Command in SmartRF Studio Figure 2-3 Exporting the Advanced TX Command in addition to the Standard Command in SmartRF Studio

SmartRF Studio and SysConfig are not giving the exact same settings when adding an extra command like this, so the code example is written to cover both cases. When using the advanced TX command, the length byte must be manually written to the packet together with the payload, and the .pktLen field of the command must include both the length field and the payload length. A code example is shown below.

1:  //---------------------------------------------------------------------------------------------
2:  // Transmit Standard Packet Format with CMD_PROP_TX_ADV (1 Length Byte)
3:  //---------------------------------------------------------------------------------------------
4:
5:  // Defines
6:  #define PAYLOAD_LENGTH 3 // Max 255 bytes
7:  #define LENGTH_FIELD   1
8:
9:  uint8_t packet[LENGTH_FIELD + PAYLOAD_LENGTH];
10:
11: static RF_Object rfObject;
12: static RF_Handle rfHandle;
13:
14: void *mainThread(void *arg0)
15: {
16:     RF_Params rfParams;
17:     RF_Params_init(&rfParams);
18:
19:     RF_cmdPropTxAdv.numHdrBits = 0x0; // Settings that must change to support 
20:                                       // the standard packet format
21:
22:     RF_cmdPropTxAdv.pktLen = LENGTH_FIELD + PAYLOAD_LENGTH; // Application specific settings
23:     RF_cmdPropTxAdv.pPkt = packet;                          
24:
25:     // Settings to modify if going from a PHY that uses the standard TX command 
26:     // to use the advanced TX command
27:     RF_cmdPropTxAdv.condition.rule = 0x1;
28:     RF_cmdPropTxAdv.pktConf.bUseCrc = 0x1;
29:
30:     rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup,
31:                        &rfParams);
31:     RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
32:
33:     while(1)
34:     {
35:         //-------------------------------------------------------------------------------------
36:         // Could be placed outside the while(1) since the packet does not change
37:         packet[0] = PAYLOAD_LENGTH;
38:
39:         for (uint16_t i = 1; i < (LENGTH_FIELD + PAYLOAD_LENGTH); i++)
40:         {
41:             packet[i] = i;
42:         }
43:         //-------------------------------------------------------------------------------------
44:         RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTxAdv, RF_PriorityNormal, NULL, 0);
45:         RF_yield(rfHandle);
46:         usleep(500000);
47:     }
48: }