SBOU274 December 2021 OPT3004
To quickly start using the device, click the "Operation Select" dropdown and select "Continuous" to bring the device out of power down mode. Then click "Start Capture" to begin data capture. The green LED on the motherboard will turn off. Lux data will appear above the lux plot as shown. The plot will also start to populate with the device lux readings.
If the GUI is not responsive, check the other Latte scripts window, which is minimized by default. If the message "Operation I2C Register Read for command [REGRx01] Failed." is displayed this means that the OPT3004 IC or coupon is not detected by the motherboard. Ensure the coupon is plugged in and properly oriented.